How to restore nxh2280 through LPCXpresso ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to restore nxh2280 through LPCXpresso ?

401 Views
esgbaek
Contributor I

Hi.

We bought NxH2280 development kit - there are 3 NxH2280 development boards.

One out of 3 seems to have some troubles - I am not sure whether hardware or software problem.

I have just evaluated one board for few days - project debug/ firmware programing etc.

After that, one board seems not work, because I have debugged through LPCXpresso.

it can not get HostApi_GetVersion(&tagOnlyParams, &getVersionResult);

- NxH2280 seems stay Bootloader always or not work in deed.

therefore I 've read your document to store nxh2280 and did it following procedure

1. Build "Audio48KHz" and Debug on LPCXpresso.

2. Move SLIDER3 to up to program nxh2280 and run Audio48Khz project.

3. After finish programming EEPROM of nxh2280, move SLIDER3 down and power cycle.

( of course IIC jumper connected between LPC1115 and nxh2280).

4. Debug again and it always stay while() loop.

     - it should work after step4, so I think it could be hardware problem.

 do
 {
  /* Give the device time to boot from EEPROM */
  BusyWaitMilliseconds(100);
#if (0)
  int r = HostApi_GetVersion(&tagOnlyParams, &getVersionResult);
#else
  HostApi_GetVersion(&tagOnlyParams, &getVersionResult);
#endif

 } while ((getVersionResult.type & 0x3) != 1);

please advise how to solve this problem.

Labels (2)
0 Kudos
1 Reply

242 Views
lpcxpresso_supp
NXP Employee
NXP Employee

Unfortunately the LPCXpresso IDE team have no direct experience of NxH2280. I would recommend that you consult with your distributor or designated Field Application Engineer.

Regards,

LPCXpresso Support

0 Kudos