How to properly wire the Ethernet connector 1769/1768?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to properly wire the Ethernet connector 1769/1768?

678 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by SSzretter on Tue Sep 06 16:07:03 MST 2011
I am getting started with the LPC 1769 unit and want to set up some simple ethernet communications.  I found the EasyWeb example project, but I am trying to verify how exactly the ethernet port is wired up.

Is there anything required beyond simply wiring the pins on the LPC unit to the corresponding pins of a female RJ45 jack, OR are there additional components required (coils?) as suggested on this page: http://vebug.com/lpcxpresso
?
0 Kudos
1 Reply

663 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Tue Sep 06 16:12:15 MST 2011
All you need is

#1 a MagJack :confused:

#2 about 10 minutes :)

See: #9 of  http://knowledgebase.nxp.com/showthread.php?t=1499
0 Kudos