LPCX support schrieb:
I'm not sure exactly what you changing parsers is meant to achieve. But the last version of LPCXpresso IDE (v8.2.2) was released a year or so before Mac OS 10.13 (High Sierra), so has never been tested on that OS.
Hi support,
the question intended more what does the parsers do and what parser do I have to choose. I still try to find out, what could have gone wrong ... Your mentioned aspect seems to be the only reason for typical crashes. Anyway, thanks for the hint!
MCUXpresso IDE, which replaced LPCXpresso IDE back in 1Q2017, is currently based on the Eclipse "Neon" framework - which is now know to have issues on Mac OS 10.13. We believe that such issues to be fixed in our next MCUXpresso IDE release (which will use Eclipse "Oxygen" framework). In the meantime, a user has produced a patch of one of part of the underlying framework which seems to resolve the issues running MCUXpresso IDE on Mac OS 10.13:
https://community.nxp.com/message/977463?commentID=977463#comment-970026
The user said the file just has to be droped into the plug-ins Folder. That's it? No manual updating of the preferences??
I'd like to use the LPC1115. I could not find any Information that this µC and the SDK for the board is supported by MCUXpresso! The list does not show this µC the old SDK for the controller/boad.
Thanks for reply!
Andreas