GDB simulator

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

GDB simulator

930 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by micronpn on Thu May 27 21:36:57 MST 2010
Is there any possibility to run an application without a real hw target using LpcXpresso IDE (i.e. like a simulator)?
If it is not possible, is it possible with RedCode3 IDE?

Original Attachment has been moved to: 1100422_output_v3.6.2.txt.zip

0 项奖励
回复
4 回复数

843 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Tue Jul 17 10:43:33 MST 2012
No, there are still no plans to add support for a simulator to the LPCXpresso IDE.

For very little money, LPCXpresso boards provide much more functionality than a simulator.

Regards,
CodeRedSupport
0 项奖励
回复

843 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by frame on Mon Jul 16 07:12:19 MST 2012
Other toolchains do have a simulator - both Keil uVision and CrossWorks have this feature, for instance.
The usability is however limited, except you refrain from using peripherals...
0 项奖励
回复

843 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by irven on Mon Jul 16 00:58:36 MST 2012
I am interested in a simulator, too.
Are there some plans to integrate it in the future?
It’s because here, at the University, we want to give the students the opportunity to test their programs hat home before they have to go to the laboratory and check if it´s working.
And the lab has only limited places for students.
0 项奖励
回复

843 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Thu May 27 23:47:33 MST 2010
Sorry, it is no on both questions - there is no simulator. Why do you want one?
0 项奖励
回复