Hello Community, I'm new here, however I have been searching online for solutions and have attempted several things and nothing has worked yet.
Symptoms:
It appears to me that lpcxpresso is somehow failing to start the server. The issue with my workaround is that once I stop the debug it kills the redlinkserv process and I have to relaunch it each time I run debug. I don't want to have to do that.
Thanks in advance!
I'm running LPCXpresso v8.2.0 [Build 647] [2016-07-18]
I'm sorry to hear that you are still having problems.
Can you please try switching to a completely new workspace, create a new "Hello world" project for your target MCU using the new project wizard, then try debugging that. Can you then successfully start a debug session, or do you still need to start Redlinkserver manually?
Something else to try would be to remove any non-essential USB devices from your system. And if you are using a dock of some description, try starting a debug session when not docked.
If you are still having problems, can you please confirm the exact version of Windows that you are using (and also whether this is an English or another local? Can you also ZIP up and post the .metadata\.log file from within your new workspace directory.
Regards,
LPCXpresso Support
The window pops back up, empty as in the first image above. Once I run redlinkserv from the command prompt I can click search for linkserveragain and it will work.
When I click search for emulator, it behaves the same way. No options until I launch redlinkserv manually.
This is still a very big problem. Thanks in advance for your help.