Content originally posted in LPCWare by matys4877 on Mon Sep 07 02:57:31 MST 2015
Hello.
I noticed that programming speed during "program flash" is over 5MHz. It's to much for me and 50% of attempt return error. I successfully changed wirespeed to 1MHz when debugging and it works well. I add -s 1000 to additional options in "program flash" dialog, but nothing has changed. I use home made cable for connection to my custom target. As emulator I use cmsis-dap from lpcxpresso54102. For local target on lpcexpresso board it works well but it seems that for my connection cable this speed is too much.
My system:
LPCXpresso v7.9.0 [Build 455] [2015-07-23]
Ni: LPCXpresso RedlinkMulti Driver v7.9 (Jul 23 2015 14:20:59 - crt_emu_cm_redlink build 468)
Pc: ( 0) Reading remote configuration
Pc: ( 5) Remote configuration complete
Nc: Probe Firmware: LPC-Link-II CMSIS-DAP (NXP)
Ubuntu 14.04
Best regards
Mateusz