Content originally posted in LPCWare by dragilla on Fri Jan 13 07:53:10 MST 2012
Hello,
I know I/O's are 5V tolerant in lpc1769. But in the UM there is this sentence:
"Crystal pins, power pins, and reference voltage pins are not 5V tolerant. In
addition, when pins are selected to be A to D converter inputs, they are no longer 5V tolerant and must be limited to the voltage at the ADC positive reference pin (VREFP)."
The question is: if I use a pin as CAP input is it 5V tolerant? I'm not sure of the mechanisms of ADC, maybe it is used when CAP is used - also I don't know what's crystal pin (the word crystal appears only once in the UM) or power pin (power supply, vbatt, etc?). Help me out a bit please.
regards,
--
Luke