Status bar shortcuts

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Status bar shortcuts

1,645件の閲覧回数
lpcware-support
Senior Contributor I

The 'Status Bar', at the bottom of the LPCXpresso IDE, has a useful set of hot links looking something like the image below:

146581_146581.pngstatusbar.png

  • Hover over the project name to reveal the full system path to your project or workspace.

  • Click on the project name or workspace name and a file browser window will open.

  • Control-click on the project name or workspace name and a command prompt (Terminal, Console) window will open.

  • Click on the Processor/Microcontroller Vendor name, and a browser window will open at their site.

  • Click on the Processor/Microcontroller Part Number, and a browser window will open at a page describing the part.

  • Control-click on the Processor/Microcontroller Part Number, and the MCU Settings dialog in Project Properties will open.

Note : You can also open a command prompt or a file browser window from the Utilities entry of the Project Explorer view's context sensitive, right-click, menu.

Submitted on Thu, 2016-03-17 06:15

ラベル(1)
タグ(2)
0 件の賞賛
返信
0 返答(返信)