what this line of datasheet means?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

what this line of datasheet means?

跳至解决方案
1,662 次查看
navidansari
Contributor III

hi

Untitled.png

it says other pins have limitation of VDD+.5 

what pins are other pins?

im using usart1 of lpc1768

can p2.1 recieve 5V signal and not break?

in what page of datasheet says it can or it can not?

标签 (1)
1 解答
1,538 次查看
soledad
NXP Employee
NXP Employee

Hi,

Please check the table 5(pin description) from the datasheet below:

http://www.nxp.com/docs/en/data-sheet/LPC1769_68_67_66_65_64_63.pdf 

In this table you can find a note about if this pin is 5v tolerant.

pastedImage_2.png

pastedImage_3.png

In addition please check the table 8. (static characteristics)

pastedImage_4.png

I hope this helps,


Have a great day,
Soledad

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
1,539 次查看
soledad
NXP Employee
NXP Employee

Hi,

Please check the table 5(pin description) from the datasheet below:

http://www.nxp.com/docs/en/data-sheet/LPC1769_68_67_66_65_64_63.pdf 

In this table you can find a note about if this pin is 5v tolerant.

pastedImage_2.png

pastedImage_3.png

In addition please check the table 8. (static characteristics)

pastedImage_4.png

I hope this helps,


Have a great day,
Soledad

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,538 次查看
navidansari
Contributor III

thanks allot

0 项奖励
回复