what is the Frame format of I2s(integrated sound).

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

what is the Frame format of I2s(integrated sound).

3,190件の閲覧回数
saikrish417
Contributor II

 is there any start and stop conditions ?

can any one help me ?

ラベル(1)
タグ(2)
2 返答(返信)

2,975件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

A sampling of frame slot formats are shown in the following figures. This is not an exhaustive set of possibilities, but shows the various frame formatting concepts. Note that slot identifications are illustrative only, data positions are flexible and there are no predefined slots for the hardware.

pastedImage_1.png

pastedImage_2.png

pastedImage_3.png

You can find more information in the following link: 

https://www.sparkfun.com/datasheets/BreakoutBoards/I2SBUS.pdf 

 

Have a great day,
Sol

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,975件の閲覧回数
saikrish417
Contributor II

hai ,

Thank you for sharing information .

My doubt is ,how Slave communicate with Master i2s ? is it single master or single slave concept or multi master concept is there or not .

how Master own bus ?

regards,

s.krish

0 件の賞賛
返信