what is the Frame format of I2s(integrated sound).

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

what is the Frame format of I2s(integrated sound).

3,442 Views
saikrish417
Contributor II

 is there any start and stop conditions ?

can any one help me ?

Labels (1)
Tags (2)
2 Replies

3,227 Views
soledad
NXP Employee
NXP Employee

Hi,

A sampling of frame slot formats are shown in the following figures. This is not an exhaustive set of possibilities, but shows the various frame formatting concepts. Note that slot identifications are illustrative only, data positions are flexible and there are no predefined slots for the hardware.

pastedImage_1.png

pastedImage_2.png

pastedImage_3.png

You can find more information in the following link: 

https://www.sparkfun.com/datasheets/BreakoutBoards/I2SBUS.pdf 

 

Have a great day,
Sol

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,227 Views
saikrish417
Contributor II

hai ,

Thank you for sharing information .

My doubt is ,how Slave communicate with Master i2s ? is it single master or single slave concept or multi master concept is there or not .

how Master own bus ?

regards,

s.krish

0 Kudos
Reply