uip dhcp probelm

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

uip dhcp probelm

841 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by cseb on Tue Jul 14 15:18:11 MST 2015
Hi all,
I have strange problem about uip tcp ip stack, dhcp module. At initialization the code can not return from function of "uip_setethaddr (mymac)". I can not understand the problem. My whole main file is like below and i have specified the problem with comment:

/*

#include "lpc17xx.h"
#include <stdio.h>
#include <string.h>
#include "lpc17xx_emac.h"
#include "timer.h"

#include "uip.h"
#include "uip_arp.h"
#include "tapdev.h"


struct uip_eth_addr mymac = { {MYMAC_1, MYMAC_2, MYMAC_3, MYMAC_4, MYMAC_5, MYMAC_6} } ;
char ipstring [20];

#define BUF ((struct uip_eth_hdr *)&uip_buf[0])

unsigned char *Key;
char buf[512];
/*--------------------------- uip_log ---------------------------------*/

void uip_log(char *m)
{
  //printf("uIP log message: %s\n", m);
}


/*--------------------------- main ---------------------------------*/

int main(void)
{
unsigned int i;
uip_ipaddr_t ipaddr;/* local IP address */
struct timer periodic_timer, arp_timer;
GPIO4->FIODIR   |= 1 << 29;
GPIO1->FIODIR = (1 << 25);
// system init
SystemInit();                                      /* setup core clocks */

// clock init
clock_init();
// two timers for tcp/ip
timer_set(&periodic_timer, CLOCK_SECOND / 2); /* 0.5s */
timer_set(&arp_timer, CLOCK_SECOND * 10);/* 10s */

// ethernet init
tapdev_init();

// Initialize the uIP TCP/IP stack.
uip_init();

 

uip_setethaddr (mymac);//--->> here the code does not return and the led does not toggle below
        GPIO1->FIOPIN ^=(1<< 25);// led does not toggle

// Start DHCP to get IP address
dhcpc_init(&mymac,6 );

 dhcpc_request();

// Initialize the HTTP server, listen to port 80.
httpd_init();
GPIO1->FIOPIN ^=(1<< 25);
while(1)
{
 /* receive packet and put in uip_buf */
uip_len = tapdev_read(uip_buf);
    if(uip_len > 0)/* received packet */
    { 
      if(BUF->type == htons(UIP_ETHTYPE_IP))/* IP packet */
      {
      uip_arp_ipin();
      uip_input();


if(uip_len > 0)
{
uip_arp_out();
tapdev_send(uip_buf,uip_len);
//GPIO1->FIOPIN ^=(1<< 25);
}
}

/* If the above function invocation resulted in data that
         should be sent out on the network, the global variable
         uip_len is set to a value > 0. */
 
      
      

      else if(BUF->type == htons(UIP_ETHTYPE_ARP))/*ARP packet */
      {
        uip_arp_arpin();

      /* If the above function invocation resulted in data that
         should be sent out on the network, the global variable
         uip_len is set to a value > 0. */
      if(uip_len > 0)
        {
        tapdev_send(uip_buf,uip_len);/* ARP ack*/

      }
      }
    }
    else if(timer_expired(&periodic_timer))/* no packet but periodic_timer time out (0.5s)*/
    {
      timer_reset(&periodic_timer);
  
      for(i = 0; i < UIP_CONNS; i++)
      {
      uip_periodic(i);
        /* If the above function invocation resulted in data that
           should be sent out on the network, the global variable
           uip_len is set to a value > 0. */
        if(uip_len > 0)
        {
          uip_arp_out();
          tapdev_send(uip_buf,uip_len);
        }
      }
#if UIP_UDP
for(i = 0; i < UIP_UDP_CONNS; i++) {
uip_udp_periodic(i);
/* If the above function invocation resulted in data that
   should be sent out on the network, the global variable
   uip_len is set to a value > 0. */
if(uip_len > 0) {
  uip_arp_out();
  tapdev_send(uip_buf,uip_len);
}
}
#endif /* UIP_UDP */
     /* Call the ARP timer function every 10 seconds. */
if(timer_expired(&arp_timer))
{
timer_reset(&arp_timer);
uip_arp_timer();
}
    }
}
}







标签 (1)
0 项奖励
回复
0 回复数