rehost lpc2378

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

rehost lpc2378

1,002 次查看
mikemillsap
Contributor I

We have legacy code written for LPC2378 that we need to rehost on an LPC4088 (new part on redesigned board).

Just thought I would start here and ask if anybody has opinions on the best approach to begin with?
Has anybody out there gone through this recently?
What are the things/"low hanging fruit" that I should be concerned about first?

I am using IAR EWARM IDE.

Thanks!

标签 (3)
0 项奖励
回复
1 回复

816 次查看
b36401
NXP Employee
NXP Employee

Please note that LPC2378 and LPC4088 processors have different memory map, different interfaces and even different ARM cores.
So you need to review all code in point of processor specific.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复