"USB Device DFU" driver missing

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

"USB Device DFU" driver missing

跳至解决方案
1,375 次查看
sigmeh
Contributor I

I use MCUXpresso IDE v24.12 [Build 148] [2025-01-10] with SDK 25.03 for LPC5516 configured as in the screenshot below
sdk.png

When adding middleware USBHSD, I get an error that an SDK component is missing. When trying to add this through quickfix, I get the following error

sdk_missing.png

When clicking on the SDK entry, I can see that this component is available in the SDK.

How can I get that to work?

标签 (2)
0 项奖励
回复
1 解答
1,103 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @sigmeh 

Please update the Config tools plugin in IDE by checking for updates (Help > Check for Updates).

However the update site is not enabled by default and must be enabled:

Alice_Yang_0-1745893581347.png

 

BR

Alice

 

 

 

在原帖中查看解决方案

0 项奖励
回复
6 回复数
1,104 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @sigmeh 

Please update the Config tools plugin in IDE by checking for updates (Help > Check for Updates).

However the update site is not enabled by default and must be enabled:

Alice_Yang_0-1745893581347.png

 

BR

Alice

 

 

 

0 项奖励
回复
1,269 次查看
sigmeh
Contributor I

@Alice_Yangany updates on that? Current versions are not working, previous are, even with only USB checked when generating.

0 项奖励
回复
1,214 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @sigmeh 

Thank you for your patience. 

It is the same with yours on my side. I have escalated it to the MCUXpresso development team for further investigation.  I will keep you updated as soon as there is any progress.

Thank you.

 

BR

Alice

0 项奖励
回复
1,352 次查看
sigmeh
Contributor I

I generated the SDK with everything checked but still having issues, even with a completely fresh project.

sdk_error.png

Also other peripherals have issues with adding the drivers.

0 项奖励
回复
1,343 次查看
sigmeh
Contributor I
Just also tested with 11.9.1 and SDK 2.16 and there it works for me.
0 项奖励
回复
1,369 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @sigmeh 

Please choose all the drivers when downloading the SDK as shown below. 

331.png

If you still encounter an issue, please take a screenshot or record a video to show how to reproduce the issue. I will checking it on my end. Thank you.

 

BR

Alice

0 项奖励
回复