"Flash_VerifyErase" does not work on PRINCE regions

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

"Flash_VerifyErase" does not work on PRINCE regions

878件の閲覧回数
awseiger
Contributor I

I have been using Flash_VerifyErase() to ensure I do not read an erased flash page and cause a hard fault. This has been working reliably until I turned on PRINCE flash encryption.

For some reason, Flash_VerifyErase() does not detect an erased region of PRINCE flash and causes a hard fault when I perform a read. The function Flash_read() does not appear to work, so as it stands I do not have a way to ensure I do not hard fault while reading Flash.

Is there a different function for detecting PRINCE erase? How can I prevent hard faulting when PRINCE is enabled?

0 件の賞賛
返信
2 返答(返信)

868件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Alexander,

Can you tell us the part number you are using? Do you use LPC55xx family?

Anyway, I suggest you refer to AN12527.pdf and AN12527SW.zip which can be downloaded from the following link:

https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mc...

 

If you still have issue, pls post all your code so that we can have a review.

BR

Xiangjun Rong

0 件の賞賛
返信

859件の閲覧回数
awseiger
Contributor I

Yes, this is for the LPC55S69, version 1B silicon - sorry I forgot that information before!

Please see my code, attached below. The commented portion is the recommended way to do Flash reads, but this section of code no longer works when PRINCE is enabled. Before I enabled PRINCE, I had this commented block inside the "else if" where the memcpy now lives.

	status_t status = FLASH_VerifyErase(&flash_instance, addr, PflashPageSize);

	if(status == kStatus_Success)
	{
		memset(data, 0xFF, len);
		return len;
	}
	else if(status == kStatus_FLASH_CommandFailure)
	{
		memcpy(data, (void*)addr, len);
	}
	else
	{
		return -1;
	}

//	status = FLASH_Read(&flash_instance, addr, data, len);
//
//	if(status == kStatus_FLASH_EccError)
//	{
//		memset(data, 0xFF, len);
//		return len;
//	}
//	else if(status != kStatus_Success)
//	{
//		return -1;
//	}
0 件の賞賛
返信