new created project file is not working on my lpc board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

new created project file is not working on my lpc board

1,160 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by chethan kumar on Tue Jul 29 01:37:59 MST 2014
Hi,

i am new to lpcexpresso IDE,I have installed LPCXpresso v6.1.4_194 tool and i want to work on FreeRTOS so i get the lpc1768 source example from freertos.org attached here that zip file and  also when i am going to use that examples and within that example main.c file i can change the code  build it and burn to my lpc board its is working fine but when i go to create new project, build it and burn to my lpc board it wont response may be problem in creating new project i don't exactly but main.c code same in both project,even i didn't get  led blinking  through gpio also.

i hope u understand my problem and please give me the solution

thank u in advance for your reply.....


Regards,

chethan kumar

Original Attachment has been moved to: source-code-for-LPC17xx-examples.rar

Labels (1)
0 Kudos
Reply
2 Replies

1,120 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by chethan kumar on Wed Jul 30 00:12:35 MST 2014

Hi,
    Thanks for your reply....
  I changed IDE version as per you are mentioned above in this version i couldn't work with lpc examples also (attached .rar file above). and i worked on LPCOPEN example freertos_blinky porject i didnt get any result. previous version IDE what i said everything is fine (if i work within the example project)only the problem is when i go to create ne project it wont work but in this version i didn't get the result with even examples also.



Regards,

chethan kumar
0 Kudos
Reply

1,120 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Tue Jul 29 03:16:53 MST 2014
Get LPCXpresso 7.30 :
[list]
  [*]http://www.lpcware.com/lpcxpresso/download
[/list]
Download LPCOpen for LPC17xx from :
[list]
  [*]http://www.lpcware.com/content/nxpfile/lpcopen-software-development-platform-lpc17xx-packages
[/list]

And try using the FreeRTOS example include as part of LPCOpen.

I would also strongly suggest that before you go any further, you read the LPCXpresso User Guide, and watch the "Rapid Embedded Development…" video at:

http://www.lpcware.com/lpcxpresso

Regards,
LPCXpresso Support
0 Kudos
Reply