lwip_tcpecho demo cannot work on LPCXpresso4337

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

lwip_tcpecho demo cannot work on LPCXpresso4337

1,013件の閲覧回数
yuanbinzhou
Contributor II

Hi all,

I used lwip_tcpecho project downloaded from LPCOpen Software for LPC43XX|NXP  to test Ethernet driver on LPCXpresso4337 board. When I successfully compiled the project and downloaded it into the LPCXpresso board, I connected the board to PC using RJ45 interface. However when I used 'ethtool' command(in Linux) to test whether Ethernet device has been connected, not any devices have been found(I has successfully seen Ethernet device using other board ).  When we use wireshark to detect whether PC has received packets from board, not any packets have been found. On the UART output, I always saw "TP ARP output". Any ideas on how to solve it? What can I do in the next step?

ラベル(1)
0 件の賞賛
返信
1 返信

869件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

This example requires a LAN connection, the board needs to be connected to a LAN. You can use a router, connect the PC and board to the router.

I hope this helps!!


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信