Hello everyone. I am a new user of the NXP chips (coming from the PICs). I have doubts about what happens at the reset. In the pics on reset, the flash memory instruction is executed at address 0x0:
Line Address Opcode Label Disassembly
1 00000 040200 goto _reset
2 00002 000000 nop
3 00004 0029FC _DefaultInterrupt
4 00006 0029FC _DefaultInterrupt
Does the same thing happen in the lpc24xx chips? Reading the manual would seem so, but I can not figure out if the address 0x0 is related to the flash memory (lpc2468):
Disassembly
0x0: 0x18 DC8 24; '.'
Region $$ Table $$ Base:
Region $$ Table $$ Limit:
__vector:
0x1: 0xf0 DC8 240; '.'
0x2: 0xe59f DC16 58783; '..'
0x4: 0xe59ff018 PC LDR, [PC, # 0x18]; Abort_Handler
0x8: 0xe59ff018 PC LDR, [PC, # 0x18]; Abort_Handler
0xc: 0xe59ff018 PC LDR, [PC, # 0x18]; Abort_Handler
At address 0x0 appears:
0x0: 0x18 DC8 24; '.'
This does not seem like a "goto"...