lpcopen_2_20 "SCT_PWM" no library file. helpe me!

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

lpcopen_2_20 "SCT_PWM" no library file. helpe me!

1,333 次查看
9218sky
Contributor II

Hi

from NXP web download surce code, opend project problem:

project index as follow:

"lpcopen_2_20_keil_iar_keil_mcb_1857\applications\lpc18xx_43xx\keil\keil_mcb_1857\periph\sct_pwm"

build on MDK error: 

.\keil_output\sct_pwm.axf: error: L6002U: Could not open file ..\..\..\..\..\..\software\lpc_core\lpc_board\boards_18xx\keil_mcb_1857\keil_output\core_m3\lib_lpc_board_keil_mcb_1857.lib: No such file or directory

project picture see accessories.

Thanks.

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

1,152 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi 9218 sky,

   Please follow my step:

1. open periph_examples in folder:lpcopen_2_20_keil_iar_keil_mcb_1857\applications\lpc18xx_43xx\keil\keil_mcb_1857

pastedImage_1.png

2. Build lib_lpc_chip_18xx and lib_lpc_board-keil_mcb_1857 two libs at first:

pastedImage_2.png

3

pastedImage_3.png

No error.

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复