lpc3240 download to nandflash

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

lpc3240 download to nandflash

1,884 次查看
243329283
Contributor I

lpc 3240 , how can I download .hex to nandflash ? (No OS ,standalone),thanks a lot

标签 (3)
0 项奖励
回复
3 回复数

1,688 次查看
soledad
NXP Employee
NXP Employee

Hi, 

 Please be aware that the LPC324 is not recommended for new design as is shown on the following link:
https://www.nxp.com/part/LPC3240FET296?lang=en&lang_cd=en&

Because of this, the support of this part is limited.

Regarding your issue, please check the following link: 

https://community.nxp.com/docs/DOC-330828

I hope this helps, 

Regards 

Sol 

0 项奖励
回复

1,688 次查看
243329283
Contributor I

Hi, Sol. Thanks for your advice a lot . 

Now my question is that : I have a lpc3240 microcontroller base band board,I do not get a lpc32x0 phythec or other development boards. But i have the kickstart loader project . How can I place the kickstart loader that it could   as the "primary boot image"?? Where should the kickstart loader be placed? IS that the block 0 page 1 of the nandflash?  

0 项奖励
回复

1,688 次查看
soledad
NXP Employee
NXP Employee

Yes,  this should be in the very first Block and Page of the NANDFLASH.

0 项奖励
回复