i2c terminal

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i2c terminal

1,798 次查看
aravindpb5009
Contributor III

hai

i am using lpc824 mcuxpresso IDE . If i used the UART communication i can see the o/p in the serial terminal,but i have one doubt if i used I2C means in which terminal i can see the o/p  plz let me  know  the solution 

Thanks & Regards 

Aravind P

标签 (1)
0 项奖励
回复
2 回复数

1,747 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Aravind,

As you know that the PC has RS232 port or USB virtual COM  port, which enable user to display message transmitted/received via uart via Hyperterminal or other tools run on PC. But the PC has not I2C interface, but there are devices which can transform I2C protocol to USB. I just searched on Google, this is the I2C to USB devices, I suppose there is tools run on PC, which enable user to transmit/receive I2C data between PC and board.

World's Smallest Adapter Module | USB to SPI - Nano River Tech 

Hope it can help you

BR

XiangJun Rong

0 项奖励
回复

1,747 次查看
aravindpb5009
Contributor III

thanks for your assistance 

0 项奖励
回复