hello, i have two LPC2364 placed on a board,
i want to connect them via Ethernet directly without using of two physical chip.
is it possible? and what is solution?
thanks in advance.
Hi,
You could directly connect both Ethernet devices without a PHY, connecting TX to RX lines and RX to TX lines. For additional details, you could refer to the following Community link:
https://community.nxp.com/thread/316374
Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------