Hi
my project runinto hardfault, the info below:
Stack:
Thread #1 57005 (Suspended : Signal : SIGTRAP:Trace/breakpoint trap)
HardFault_Handler() at semihost_hardfault.c:72 0x1da54
<signal handler called>() at 0xfffffff1
xTaskIncrementTick() at tasks.c:2,705 0x1a4c4
SysTick_Handler() at port.c:447 0x19510
<signal handler called>() at 0xffffffed
prvPortStartFirstTask() at port.c:217 0x19304
xPortStartScheduler() at port.c:329 0x19412
Faults info:
Active faults @\amazon-freertos\FreeRTOS\tasks.c line 2707
Bus Fault (BFSR)
BFARVALID (7) BusFault Address Register (BFAR) valid flag
PRECISERR (1) Precise data bus errorHard Fault (HFSR)
FORCED (30) Indicates a forced hard fault, generated by escalation of a fault with configurable priority that cannot be handled, either because of priority or because it is disabled
Fault Status RegistersIPSR 0x00000003 Exception Status Register (Hard Fault)
CFSR 0x00008200 Configurable fault Status Register
MMSR 0x00000000 Memory Manage fault Status Register
BFSR 0x00000082 Bus fault Status Register
UFSR 0x00000000 User fault Status Register
HFSR 0x40000000 Hard fault Status Register
DFSR 0x00000001 Debug fault Status Register
MMAR 0x3805C938 Memory Manage fault Address Register
BFAR 0x3805C938 Bus fault Address Register
AFSR 0x00000000 Auxiliary fault Status Register
Stacked Registers (SP LR/EXC_RETURN=0xfffffff1)R0 0x00000003
R1 0x2001CCAC
R2 0x0E003307
R3 0x3805C938
R12 0x000000AA
LR 0x00018E25 SysTick_Handler() @ \amazon-freertos\FreeRTOS\portable\port.c line 451
PC 0x00019DD8 xTaskIncrementTick()
PSR 0x2100000FSP 0x20027F90
my project info:
MCU:LPC54606
OS:FreeRTOS
Middleware:Lwip with SDK
SDK:2.4.1
Interrupt used: Enet by LWIP with Priority 6
PINT0,PINT1 with no Priority settings, default priority?
peripherals used: flexcomm0(SPI poll mode), flexcomm3(SPI poll mode),
5 GPIOs
the FreeRTOSConfig.h settings as below:
#define configUSE_PREEMPTION 1
#define configUSE_TICKLESS_IDLE 0
#define configCPU_CLOCK_HZ (SystemCoreClock)
#define configTICK_RATE_HZ ((TickType_t)100)
#define configMAX_PRIORITIES 5
#define configMINIMAL_STACK_SIZE ((unsigned short)100)
#define configMAX_TASK_NAME_LEN 10
#define configUSE_16_BIT_TICKS 0
#define configIDLE_SHOULD_YIELD 1
#define configUSE_TASK_NOTIFICATIONS 1
#define configUSE_MUTEXES 1
#define configUSE_RECURSIVE_MUTEXES 1//0 liang 5.23
#define configUSE_COUNTING_SEMAPHORES 1
#define configUSE_ALTERNATIVE_API 0 /* Deprecated! */
#define configQUEUE_REGISTRY_SIZE 8
#define configUSE_QUEUE_SETS 0
#define configUSE_TIME_SLICING 1//
#define configUSE_NEWLIB_REENTRANT 0
#define configENABLE_BACKWARD_COMPATIBILITY 1
#define configNUM_THREAD_LOCAL_STORAGE_POINTERS 5
#define configUSE_APPLICATION_TASK_TAG 0
... ...#ifdef __NVIC_PRIO_BITS
/* __BVIC_PRIO_BITS will be specified when CMSIS is being used. */
#define configPRIO_BITS __NVIC_PRIO_BITS
#else
#define configPRIO_BITS 3 /* 15 priority levels */
#endif
/* The lowest interrupt priority that can be used in a call to a "set priority"
function. */
#define configLIBRARY_LOWEST_INTERRUPT_PRIORITY 7//((1U << (configPRIO_BITS)) - 1)//7
/* The highest interrupt priority that can be used by any interrupt service
routine that makes calls to interrupt safe FreeRTOS API functions. DO NOT CALL
INTERRUPT SAFE FREERTOS API FUNCTIONS FROM ANY INTERRUPT THAT HAS A HIGHER
PRIORITY THAN THIS! (higher priorities are lower numeric values. */
#define configLIBRARY_MAX_SYSCALL_INTERRUPT_PRIORITY 2//liang 5.23
/* Interrupt priorities used by the kernel port layer itself. These are generic
to all Cortex-M ports, and do not rely on any particular library functions. */
#define configKERNEL_INTERRUPT_PRIORITY (configLIBRARY_LOWEST_INTERRUPT_PRIORITY << (8 - configPRIO_BITS))
/* !!!! configMAX_SYSCALL_INTERRUPT_PRIORITY must not be set to zero !!!!
See http://www.FreeRTOS.org/RTOS-Cortex-M3-M4.html. */
#define configMAX_SYSCALL_INTERRUPT_PRIORITY (configLIBRARY_MAX_SYSCALL_INTERRUPT_PRIORITY << (8 - configPRIO_BITS))
I have seen this post:FreeRTOS bug in xQueueGenericSendFromISR ?
I thinks they say wrong in the post ,
"Content originally posted in LPCWare by alramlechner on Fri Aug 07 13:28:29 MST 2015
just found it. IRQ priority, which uses FreeRTOS API, must have lower priority than SysTick ... "
actually all other IRQ priority should have higher priority than Systick(configKERNEL_INTERRUPT_PRIORITY), and lower than configLIBRARY_MAX_SYSCALL_INTERRUPT_PRIORITY (http://www.freertos.org/a00110.html#kernel_priority).
my project follow this rule , but hardfault still. i don't know why.
Hi, LiangChen,
As you know that the Cortex-M4 use the follow IPR register format for each external interrupt source:
For example, the interrupt priority of IP_CTIMER0 for LPC546xx are located at bit21~23, it's priority is from 0 to 7(from 3b'000 to 3b'111), the 3b'000 is of highest priority, the 3b'111 is of lowest priority. The configMAX_PRIORITIES is set up as 5 using the line in FreeRtos system:
#define configMAX_PRIORITIES 5
So for your own peripheral interrupt source, you have to set priority of your own peripheral interrupt source lower than 5 level. In other words, set the IPR register value greater than 5. For example, you want to use IP_TIMER0 module interrupt, and post an event, so you have to set up the IP_CTIMER0 bits(bit21~23) for example 6, 3b'110, it is okay.
Hope it can help you
BR
XiangJun Rong
Hi Rong
thanks for helping.
In my project:configMAX_PRIORITIES = 2,configKERNEL_INTERRUPT_PRIORITY =7.
PINT0、PINT1 Priority =4 ;Enet Priority = 6;CTIMER0、CTIMER1 Priority = 4;
All other peripherals's interrupt are disabled.