emwin demo of lpc1788

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

emwin demo of lpc1788

1,001 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lgeorge123 on Tue Mar 27 02:43:54 MST 2012
I have downloaded the demo code of emwin from lpcware and run under lpc1788 , it works but I cannot change the display orientation even I alter the "  LCD_MIRROR_X,LCD_MIRROR_Y,LCD_SWAP_XY " , is it a demo program so no body can change it ??
标签 (1)
0 项奖励
回复
3 回复数

966 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by chikli on Tue Apr 10 14:05:20 MST 2012
On another thread I posted my difficulty of running the demo code of emwin from lpcware. In this thread you indicate that you are successful in running the code. Can you please assist and give me any pointers regarding difficulties or changes you made to run the demo code? I am using LPCXpresso, with an Embedded Artists 1788 board and a 4.3" LCD. What programming platform and hardware are you using? Any assistance would be greatly appreciated.
0 项奖励
回复

966 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lgeorge123 on Tue Mar 27 04:35:14 MST 2012
Thanks your reply , now I can change the orientation !!
0 项奖励
回复

966 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by drs on Tue Mar 27 03:57:34 MST 2012
You will need to change the display driver. See 30.7.5 GUIDRV_Lin in the Segger user manual for more information.
0 项奖励
回复