eRPC for NXP LPC54605 with SPI transport

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

eRPC for NXP LPC54605 with SPI transport

跳至解决方案
1,740 次查看
sevi
Contributor II

Hi,

 

I'm looking for a convinient way to create an control and data transfer interface between the NXP MCU LPC54605 and embedded petalinux.

 

In a quick test i run into missing driver like fsl_port.h which is not available for LPC54605.

Is there a way to use eRPC with this MCU?

 

Thank you

标签 (2)
标记 (1)
0 项奖励
回复
1 解答
1,730 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport
0 项奖励
回复
2 回复数
1,731 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport
0 项奖励
回复
1,723 次查看
sevi
Contributor II

Hi,

 

Thank you for the answer, the information in https://github.com/EmbeddedRPC/erpc/wiki/Getting-Started were the best starting point for me.

But the problem with the missing fsl_port.h still exists. As a workaround I created an empty fsl_port.h file to be able to completely build the code.

 

Thank you and best regards

0 项奖励
回复