drawing combo box with scroll bar and graphs in lcd

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

drawing combo box with scroll bar and graphs in lcd

631 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Elavarasan on Wed May 02 07:00:57 MST 2012
Dear all,

We are developing a System On Module (SOM) using LPC3250. We are not using any Embedded OS. We have to display a Combo Box with Scroll Bar in LCD. We are trying and it is some what displaying like Combo Box (without Scroll Bar). But still it is not 100% complete. We have to fine tune and display with Scroll Bar. Is there any reference code examples or application notes available for this? And we have to draw some Graphs also. Anyone used this kind of application already? If somebody helps on this it would be useful for us.

Thanks in Advance,
S.Elavarasan
标签 (1)
0 项奖励
回复
0 回复数