designing my board using lpc1549

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

designing my board using lpc1549

1,487 Views
emrebaltaci
Contributor I

I need to design my board using lpc1549 microprocessor. I designed the power supply part and also related part of my final thesis, but i didnt knowledge of  usage of lpc1549 lqfp64 package. Which systems must be included in my design. Can anyone lead to me?

i am also use lpcxpresso v2 schematic pdf. which parts in this schematic pdf is necessary?

Labels (1)
0 Kudos
Reply
1 Reply

1,344 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Emre,

From my understanding, you want to design LPC1549 Minimum System. Is that correct?

If so, I suggest you refer our schematic of OM13056 LPCXpresso_v2 demo board.

https://www.nxp.com/downloads/en/schematics/LPC1549_LPCXpresso_v2_schem_Rev_C.pdf 

Your design needs to include:

1. LPC1549 power supply/ground, reset circuit

2. if external clock needed, you need include external osc circuit

3. SWD interface for debug

4. ISP0, ISP1 for boot

Please note, the demo board schematic includes built in Link2 debug probe. customer board usually doean't need it, external debug probe is used instead. I suggest you get a LPC-Link2 debug probe for it.


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------