couldn't see the uart communication through the JTAG?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

couldn't see the uart communication through the JTAG?

980 次查看
aravindpb5009
Contributor III

hai 

        we are using the lpc824 controller and lpc link2 debugger , for debugging purpose we connecting through the JTAG

we  need to send send  the uart value from lpc824  to wifi module, need to know what values communicating  to lpc824 and wifi . for that  we try to open the com port which connected in jtag. But the jtag com port was not opening .let me know if its possible to open the com port which connected through jtag to lpc824 mcu

Thanks&Regards 

Aravind P

标签 (4)
0 项奖励
回复
1 回复

879 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Aravind palanisamy

LPC824 LPCXpresso V2 demo board does include VCOM. But LPC-Link2 probe currently does not support this feature.

If use LPC-Link2, Normally, user prints content to debug console or uart.


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复