clock frequency of i2c in LPC1347

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

clock frequency of i2c in LPC1347

1,878 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by sariga on Mon Mar 04 04:03:08 MST 2013
hi ,
i am new to this forum aswell as to lpc microcontrller.i'm using lpc1347 to interface an accelerometer (mma8452q) thru i2c interface which is by default in 100khz..trouble is i dont get from datasheet how to set the clock of i2c..i hav a 12MHz crystal oscillator..know how to set sclh and scll..but how to set pclki2c ? i got this formula,
and lpc1347 in standard/ fast mode (by default)

I 2 C bitfrequency =            PCLKI2C
                         ----------------------------------
                              SCLH + SCLL


sorry if i sound too silly, but plzz help..
Labels (1)
0 Kudos
Reply
1 Reply

1,678 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Paul on Wed May 08 13:39:00 MST 2013

Hello Sariga
First, you need to determine the clock to the I2C peripheral which is PCLKI2C.  Looking at Figure 3 in the UM10524 User's Manual, you will see that the clock to the I2C peripheral is the main clock divided by the system clock divider.  You didn't specify what your main clock was set to, but let's assume that you are using the PLL to bring the clock speed up to 72MHz.  Most of the time, the system clock divider (SYSAHBCLKDIV) is set to '1', so then the I2C peripheral block will also be 72 MHz.  Don't forget to enable the clock to the I2C peripheral by setting bit 5 in SYSAHBCLKCTRL to '1'.
If you want to get 100kHz from the I2C clock, the equation becomes:
SCLH + SCLL = (PCLKI2C)/(I2C bit frequency) = (72MHz)/(100kHz) = 720
So, the total of the SCLH and SCLL registers should be 720.  The easiest thing to do is split it evenly between the two, and therefore load the value 360 into each of the SCLH and SCLL registers.
The I2C specification states that the minimum clock low time for a 100kHz bus should be 4.7us while the minimum clock high time is 4.0 us.  The low and high times for this configuration will be 360/72MHz=5.0 us, so we can meet both the I2C clock low and high requirements.
Hopefully that makes things easier to understand.

0 Kudos
Reply