change PWM frequency

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

change PWM frequency

1,685 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by [email protected] on Fri Jul 26 17:56:58 MST 2013
The code below sets up a simple 2-edged PWM signal. In my application, I need to change the frequency occasionally, which is what I THINK I am doing in the main loop, but the only change is the duty cycle. That is, the frequency always remains to what it was set at the beginning (1kHz), and only the "on" duty cycle is commensurate with the 2kHz I'm switching it to.

Any ideas, anything I'm obviously forgetting here?

--J.


#include "LPC17xx.h"

float duty; 
int PWMclock; 
int PWMrate; 
float frequency; 

 
int main() 
{
    int PWMwidth, PWMhalf, PWMrising, PWMfalling;   

    duty = 50.0;
    frequency = 1000.0;
    
    PWMclock = SystemCoreClock / 4;
    PWMrate = PWMclock / frequency; 
    LPC_PINCON->PINSEL4 |= 0x00000040;                     // Set P2.3 for PWM1.4
    
    LPC_PWM1->MCR |= 0x00000002; // Reset PWM0 on match

    // Set up match registers
    LPC_PWM1->MR0 = PWMrate; // Set MR0 (PWM rate)

    LPC_PWM1->PCR |= 0x00000010; // Select double edge PWM for PWM4

    LPC_PWM1->PCR |= 0x00001000; // Enable PWM4

    LPC_PWM1->TCR |= 0x08; // Enable PWM mode
    LPC_PWM1->TCR |= 0x01; // Enable counter
 
    //pwmChg.attach_us(&pwmupdate, 100000);
 
    while (1)
    {
 
        frequency = 1000.0;
        PWMrate = PWMclock / frequency; 
        LPC_PWM1->MR0 = PWMrate; // Set MR0 (PWM rate)

        PWMwidth = (duty * PWMrate) / 100;
        PWMhalf = PWMwidth / 2;
        //PWMrising = PWMrate - PWMhalf;
        //PWMfalling = PWMhalf;
        PWMfalling = PWMrate - PWMhalf;
        PWMrising = PWMhalf;        
    
        LPC_PWM1->MR3 = PWMrising; // Set rising edge
        LPC_PWM1->MR4 = PWMfalling; // Set falling edge
    
        LPC_PWM1->LER |= 0x18; // Enable PWM Match 3 & 4 latch
    
        for (int i; i<10000000;i++){}
        
        frequency = 2000.0;
        PWMrate = PWMclock / frequency; 
        LPC_PWM1->MR0 = PWMrate; // Set MR0 (PWM rate)

        PWMwidth = (duty * PWMrate) / 100;
        PWMhalf = PWMwidth / 2;
        //PWMrising = PWMrate - PWMhalf;
        //PWMfalling = PWMhalf;
        PWMfalling = PWMrate - PWMhalf;
        PWMrising = PWMhalf;   
    
        LPC_PWM1->MR3 = PWMrising; // Set rising edge
        LPC_PWM1->MR4 = PWMfalling; // Set falling edge
    
        LPC_PWM1->LER |= 0x18; // Enable PWM Match 3 & 4 latch
        
        for (int i; i<10000000;i++){}       
        
    }
}
标签 (1)
0 项奖励
回复
0 回复数