about LPC2378 CAN sleep mode

cancel
Showing results for 
Search instead for 
Did you mean: 

about LPC2378 CAN sleep mode

376 Views
Contributor I

CAN1MOD = CAN2MOD = 0x10;

when the CAN enter sleep mode,I send one date to awake it by the other machine,it success,but later,it do  not sleep again,because the CAN BUS activity,so,it did not enter sleep mode.

  But I only send one date and then close the machine,Why the CAN bus is acticity all the time? How can I make the CAN BUS isn't activity?

QQ截图20161230115536.png

0 Kudos
1 Reply

11 Views
NXP Employee
NXP Employee

Hi,

According with your description, and the relation with your other thread:

https://community.nxp.com/thread/441666

 

It seems that there are some pending interrupts to be cleared on the CAN, so, therefore, the CAN module cannot enter sleep mode, and it is triggering a wakeup interrupt, causing that the entire MCU is not able to enter into sleep mode (that’s why you are seeing PCON=0x00 instead of 0x81 after starting the transmission).

So, in order to avoid such behavior, you should verify your CAN bus state to ensure a correct CAN termination and bus idle condition when disconnecting the other device that sends CAN data; additionally to verify the logic of the code to attend any pending interrupt and allow the module to enter into sleep mode and not causing interrupts that awakes the entire MCU from low power mode.


Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos