Zephyr USB support for LPC54114 uC

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Zephyr USB support for LPC54114 uC

2,168 次查看
mme
Contributor I

Hello

is the USB controller in LPC54114 supported with Zephyr? As far as I could investigate, the USB is based on LpcIP3511 which indeed is supported but I could not get it working or find matching examples.

Thanks for feedback.

0 项奖励
回复
7 回复数

2,093 次查看
mme
Contributor I

Hello @Alice_Yang 

Since you say that LPC54114 is supported, can you kindly provide a complete Devicetree with USB and even a basic example? Documentation is not available and you always refer to your examples, so getting one would be essential!

Thanks.

0 项奖励
回复

2,065 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @mme 

I confirmed with our SE team, the USB Devicetree doesn't support lpc54114.

If you to know additional information about Zephyr, you can create a new thread on community , and mentioned

Derek Snell <derek.snell@nxp.com> for help.

 

BR

Alice

0 项奖励
回复

2,129 次查看
mme
Contributor I

Hi @Alice_Yang 

Thank you for the link. USB is not stated on the supported features list, which is why I placed this question first hand. However, the USB Core IP3511 has Zephyr driver support, so what is missing, is a DTS/DTSI for the SOC supporting a USB Interface. Anything you can do to make this supported?

 

BR MME

0 项奖励
回复

2,122 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @mme 

1) About Zephyr detail issue, you can ask at Zephyr community, NXP’s support team actively monitors the Zephyr community to support customers with questions specific to NXP’s platforms.

https://www.zephyrproject.org/community/ 

 

2) Can you access this thread:

https://community.nxp.com/t5/Zephyr-CAS-Training/gh-p/60248

If yes, also can ask Zephyr question here.

 

BR

Alice

 

0 项奖励
回复

2,117 次查看
mme
Contributor I

Hi @Alice_Yang I can not access this trhread.

 

0 项奖励
回复

2,098 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @mme 

How abut the first thread?

https://www.zephyrproject.org/community/   

 

BR

Alice

0 项奖励
回复

2,134 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @mme 

Yes, it support:  https://docs.zephyrproject.org/latest/boards/arm/lpcxpresso54114/doc/index.html  

There is a training about Zephyr with NXP, you can have a look at:

https://community.nxp.com/t5/Zephyr-CAS-Training/Intro-to-Zephyr-with-NXP/ta-p/1282026  

 

BR

Alice

0 项奖励
回复