I observed that when I'm increase or decrease variable array size, flash size is also change.
I have seen in Flash Memory contents it shows .bss section which occupy considerable amount of Flash why .bss section comes in Flash?? It should be there in RAM section only.
I have even check linker setting in project setting but no option available?
I wonder why .bss section is mapped in SRAM and how to change it?
Maybe you could share some details about what you see?
Maybe you see the problem described here: GNU Linker, can you NOT Initialize my Variable? | MCU on Eclipse
I hope this helps,
Erich
No this is not like that.. I know basic concept of .data, .bss,..etc. If any data is initialized with any value then it considered as .data not .bss.
In my case
1) suppose array size is 256
uint8_t variable[256];
I got below memory usage in MXUXpresso
In Image Info -> Memory Usage
Program Flash - 13.47 KB
SRAM - 4.52 KB
In console window after compilation
text data bss dec hex filename
9311 64 4560 13935 366f test.axf
2) Changed array size to 1024
uint8_t variable[1024];
I got below memory usage in MXUXpresso
In Image Info -> Memory Usage
Program Flash - 14.23 KB (increased by 768)
SRAM - 5.27 KB
In console window after compilation
text data bss dec hex filename
9315 64 5328 14707 3973 test.axf
After compare above result i thought there may have some error in memory usage calculation in Image Info or something I'm missing not sure..
Result in console window is ok.
Why image Info show wrong memory usage??
Well, if you increase the array from 256 to 1024 the difference is 768. I can't see a fault neither in Image Info nor in console. Image Info has a very small difference because of the unit in kB (not really, but it looks like).
Obviously I don't understand the problem; please describe again more clearly.
I tried the same, but I have to say it is correct for me (using a K22 device):
With this
uint8_t var[256];
I get
Region Start address End address Free Used Usage (%)
PROGRAM_FLASH 0x0 0x40000 262144 254436 7708 2.94%
SRAM_UPPER 0x20000000 0x20004000 16384 13880 2504 15.28%
SRAM_LOWER 0x1fffc000 0x20000000 16384 16384 0 0.00%
FLEX_RAM 0x14000000 0x14001000 4096 4096 0 0.00%
and with this
uint8_t var[256+1024];
I get
Region Start address End address Free Used Usage (%)
PROGRAM_FLASH 0x0 0x40000 262144 254436 7708 2.94%
SRAM_UPPER 0x20000000 0x20004000 16384 12856 3528 21.53%
SRAM_LOWER 0x1fffc000 0x20000000 16384 16384 0 0.00%
FLEX_RAM 0x14000000 0x14001000 4096 4096 0 0.00%
which is what I expect.
Can you share your project here so the engineers could have a look?
Hello,
I checked your project and did the following:
Build the project and got the following results
Memory region Used Size Region Size %age Used
PROGRAM_FLASH: 4612 B 24560 B 18.78%
PRODUCT_INFO: 0 GB 16 B 0.00%
SRAM: 4288 B 16 KB 26.17%
Finished building target: bss.axf
make --no-print-directory post-build
Performing post-build steps
arm-none-eabi-size "bss.axf" ; arm-none-eabi-objcopy -v -O binary "bss.axf" "bss.bin" ; # checksum -p LPC845 -d "bss.bin"
text data bss dec hex filename
4608 4 4284 8896 22c0 bss.axf
Then, I increased txBuffer as you suggested:
And I got the results below:
Memory region Used Size Region Size %age Used
PROGRAM_FLASH: 4612 B 24560 B 18.78%
PRODUCT_INFO: 0 GB 16 B 0.00%
SRAM: 5312 B 16 KB 32.42%
Finished building target: bss.axf
make --no-print-directory post-build
Performing post-build steps
arm-none-eabi-size "bss.axf" ; arm-none-eabi-objcopy -v -O binary "bss.axf" "bss.bin" ; # checksum -p LPC845 -d "bss.bin"
text data bss dec hex filename
4608 4 5308 9920 26c0 bss.axf
It seems the bss is increased correctly, could you please clarify if you are doing something differently or if I missed something?
Best regards,
Felipe
As i told in earlier post, Console shows correct value but Image Info shows wrong value. Please compare below images with different buffer size.
With 256:
with 4096:
Hope above image is enough to describe my issue.
I just had a quick look, using the 'bss' project that you provided previously.
First comment is that the figures provide in the Memory Usage tab are those that are output by the linker when using --print-memory-usage, so it is the linker that is generating her numbers.
So, using the
U8 au8RxBuffer[4096];
I see
PROGRAM_FLASH: 4612 B 24560 B 18.78%
PRODUCT_INFO: 0 GB 16 B 0.00%
SRAM: 4288 B 16 KB 26.17%
and when using
U8 au8RxBuffer[256];
I see
PROGRAM_FLASH: 4620 B 24560 B 18.81%
PRODUCT_INFO: 0 GB 16 B 0.00%
SRAM: 448 B 16 KB 2.73%
So the only significant difference is that SRAM increases by 3840 bytes (the difference being the increase in the buffer size (4096-256).
This is using the application that you posted, with the only change being the size of auRxBuffer. What is it that you are doing that is different?
[EDIT]
Comparing the numbers shown in the Image Info view - I DO see your problem. This looks like a bug in the ImageInfo viewer @NXP - can somebody look into this?
As I said in earlier post In console tab everything is OK only issue is in Image Info tab.
compare Usage (%) in previous post where i have shown you with memory usage with different buffer size.
Region PROGRAM_FLASH should not change if i change buffer value.