Whether lpc1788 have SPIFI? If is not present, then how to me to make loading of external flash through spi/ssp?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Whether lpc1788 have SPIFI? If is not present, then how to me to make loading of external flash through spi/ssp?

1,840件の閲覧回数
alexkovtun
Contributor I

It is necessary to connect external flash as there is not enough internal memory for storage of a code. The project for work with the display 640*480.

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,616件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Alex Kovtun,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.

The SPIFI is a available on the LPC1773 device only, and you can choose some NOR-flash chip via the SPI interface, such as Winbond W25x family.

Hope it helps.

Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,616件の閲覧回数
alexkovtun
Contributor I

Attach, please, examples or materials for setting the programming algorithm SPI Flash.

0 件の賞賛
返信

1,616件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Alex Kovtun,

Thanks for your reply.

You can learn the more information about the Winbond W25 family via the link below.

Winbond - Serial NOR Flash
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信