Where's the link for joining to the discussion in order to be the 100 first individuals getting access to the LPC54608 development board (OM13092)?
申请 LPC54608开发板
1。 LPC54608开发板申请的原因: 用于多功能人机交互的设备监控系统。许多工厂都需要这个监控设备。
2。 采用LPC54608的原因:
A.多达10个串口。因为监控设备要与多个串口RS232或是RS485的设备互连,通讯。
B.有CAN通讯接口
C. 有USB接口,接U盘等待。
D.有驱动大屏的接口,方便接一个显示大屏,方便显示相关参数。
E. 需要多通道ADC,采集一些模拟参数,比如电压,电流,温度,压力等待。
F.程序比较大,数据多,需要一个强大的芯片来做,需要高主频,运算能力强的芯片。STM32F407IGT6弱于这个LPC54608
G.需要网络接口,便于远程控制。
仪表那块本来就不需要跑Linux,跑RTOS更适合,就是图形界面开发难度大一点。安全性、可靠性更高。我认为中低档车用这个方案更好!
lpc546x的高性能,似乎可以应用在车载虚拟仪表上了,是否比iMX6或iMX7价格要低一些呢?
你好!i.MX6 & iMX7是NXP的MPU,跑Linux合适。LPC5460x是MCU,跑RTOS合适。两者定位不一样。价格上LPC5460x比i.MX6/7要低。
Hi, let's start a discussion, please just post some ideas how you have used or plan to use LPC in your application!
You can find more information here: https://contact.nxp.com/lpcroadmap?elq_mid=4585&elq_cid=2408128
and here: https://community.nxp.com/community/lpc/blog/2016/12/20/get-a-free-lpcxpresso54608-development-board
Hi, thank you for the post!
by December 31, 2016, start your own discussion (put LPCXpresso54608 in your title) on our LPC community in which you share how you might use a new or existing LPC microcontroller in an application, maybe it's a new feature or product you want to try, could be something you've already created or a new idea you want to create in 2017. Be creative and have fun sharing ideas. Up to 100 submissions (non-NXP employees) will be selected to receive an LPC54608 board (OM13092).