Where is the list of Physical pin of LPC824?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where is the list of Physical pin of LPC824?

ソリューションへジャンプ
1,898件の閲覧回数
franciscopasten
Contributor I

Hi all,

I use LPC824 and i want to use the second i2c but i don't find the physical pin number to use with the function 

Chip_SWM_MovablePinAssign(CHIP_SWM_PIN_MOVABLE_T movable, uint8_t assign), then what number use in assign variable for any pin? 

Thanks

ラベル(3)
0 件の賞賛
返信
1 解決策
1,708件の閲覧回数
johanmyréen
Contributor II

PIO0_1 is pin 1, PIO0_15 is pin 15. In general, PIO0_n is pin n. See section 7.3.1 the User Manual (UM10800).

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,708件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

Please check the below information from user manual: http://www.nxp.com/docs/en/user-guide/UM10800.pdf 

pastedImage_1.png

pastedImage_3.png


Have a great day,
Soledad

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,708件の閲覧回数
franciscopasten
Contributor I

Dear Soledad, 

i have this:


 Chip_SWM_MovablePinAssign( SWM_I2C1_SCL_IO, x);
 Chip_SWM_MovablePinAssign( SWM_I2C1_SDA_IO, y);

but i don't know which numbers use in x,y for assignate PIO0_1 and PIO0_15 as SDA and SCL pins for I2C1

Do you know if there's a table with that information?

thanks 

0 件の賞賛
返信
1,709件の閲覧回数
johanmyréen
Contributor II

PIO0_1 is pin 1, PIO0_15 is pin 15. In general, PIO0_n is pin n. See section 7.3.1 the User Manual (UM10800).

0 件の賞賛
返信