Hello everyone,
I have a question regarding the usage of GPIOs of the LPCXpresso55S69 board. I have trouble finding an explanation/a picture, which GPIO routs to which output pin. Meaning, that I found the "Pins" View in the SDK:
But how do I know where e.g. PIO0_12 is on the board? I have found those two pictures, which are not helpful at all, because they don't use the same naming. So, where do I have to put my cable on my board if I want to attach it to e.g. PIO0_12? Where do I find this information? Or am I just too stupid to understand those pictures?
I would be really glad if someone could point me to the correct direction.
Best regards
Ximena
已解决! 转到解答。
Hi Ximena,
I check P18 connector, there are also other GPIO pins connected. For example PIO1_9, PIO1_10, PIO1_15, PIO1_18.
some of them are defined as input buttons. but you can also config it as gpio output.
For more see demo board UM and Schematic.
Have a nice day,
Jun Zhang
PIO0_12 was just an example, I don't really want to use it. It was just a random number!!
I only want to know the connection between the pins on my board and the ones in the "Pin" View in the SDK. Where do I find that?
I just want to get a high trigger signal at one of the GPIO pins to connect an oscilloscope. I don't care which one, just one. But I cannot find any information on how to address which pin to do so...
Hi
If you just want to test GPIO feature, LPCXpresso55S69 board provides P1_4, P1_6 and P1_7 for it.
The LEDs in this device are controlled by LPC55Sxx ports P1_4 (Blue), P1_6 (Red), P1_7
(Green) with the LEDs being illuminated when the respective LED is pulled low. Note that
these port lines are also connected to expansion connector P18.
You can check it with SDK demo code gpio_led_output. Here is pin configuration:
Hope this helps,
Jun Zhang
Hello Jun,
thanks for your answer. Yes, I want to test the GPIO feature, but not with the LEDs
So is there a GPIO that I can address in my uC-program, that routs to this P18 extension connectors that is not an LED? And if so, where can I find the exact location so I can put my cable there?
Kind regards
Ximena
Hi Ximena,
I check P18 connector, there are also other GPIO pins connected. For example PIO1_9, PIO1_10, PIO1_15, PIO1_18.
some of them are defined as input buttons. but you can also config it as gpio output.
For more see demo board UM and Schematic.
Have a nice day,
Jun Zhang