Where can I get the LPC54608 BSDL file

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where can I get the LPC54608 BSDL file

Jump to solution
1,724 Views
hugh_okeeffe
Contributor I

I need this to allow BST/JTAG testing of my LPC54608 powered product

thanks

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,555 Views
soledad
NXP Employee
NXP Employee

Hi,

Please check the attached files.


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
3 Replies
1,555 Views
hugh_okeeffe
Contributor I

Probably QFP but we may change. Is it available for both ?

Thanks Sol

0 Kudos
Reply
1,556 Views
soledad
NXP Employee
NXP Employee

Hi,

Please check the attached files.


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,554 Views
soledad
NXP Employee
NXP Employee

Hi,

Which package do then use to conduct the test? BGA or QFP?

Regards 

Sol

0 Kudos
Reply