Where can I buy a LPC4370 demoboard?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where can I buy a LPC4370 demoboard?

623 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by eTrig on Fri Mar 28 08:40:24 MST 2014
LPC4370 is a very powerful MCU, but I can't found a demo board. If I want to use this MCU, what is the best way?
Labels (1)
0 Kudos
Reply
1 Reply

597 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by arw on Sun Mar 30 19:08:46 MST 2014
Hello,
There are two ways to evaluate this chip.  The LPC4370 is designed onto the LPC-Link2 debugger.  You can actually use it as a target board for the microcontroller as well, and use one Link2 board to debug another.  Also, the oscilloscope/logic analyzer known as LabTool adds additional hardware interfaces to the Link2.  The full source code for LabTool is also released.
See these sites for details.

http://www.lpcware.com/lpclink2

http://www.embeddedartists.com/products/app/labtool.php

Cheers!
0 Kudos
Reply