Customer:www.dB-mark.com
Device:LPC5500
Our customer(www.dB-mark.com) is evaluating LPC5500 PowerQuad computing features. Customer can't find any detial description about "ret" and "ref" in below formula. Any comment for these two parameters?
Hello S.z. Liang,
I just got reply from PowerQuad expert of SE team as below:
"
"res" is usually short for "result", which is the result computed by the formula.
"ref" is usually short for "reference", which is the actually result sampled in real condition.
This accuracy computing formula is just to convert the percentage error to dB way. This is no special method here.
"
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------