What is the value of TWDCLK at the Windowed Watchdog Timer in LPC802?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

What is the value of TWDCLK at the Windowed Watchdog Timer in LPC802?

1,814 次查看
barbaramoraes
Contributor II

Hi! 

I wish to know what TWDCLK means, like in the case bellow:

pastedImage_1.png

When it talks about the minimum and maximum interval to watchdog, what means the TWDCLK, in yellow?

Best regards,

标签 (3)
标记 (3)
3 回复数

1,633 次查看
barbaramoraes
Contributor II

Thank you very much guys!!!

1,633 次查看
carstengroen
Senior Contributor II

According to the datasheet, the wdt oscillator is the "LPOsc" as far as I can tell.

And that has the following specs:

pastedImage_1.png

So the answer must be "approx 1 MHz"

1,633 次查看
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Barbara! 

The answer that Carsten Groen gave is correct. TWDCLK  is the clock of the Windowed Watchdog timer, that corresponds to the LPOsc. If you want to substitute TWDCLK  for the corresponding value you can use 1MHz.

Regards, 

Victor.