What is the value of TWDCLK at the Windowed Watchdog Timer in LPC802?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the value of TWDCLK at the Windowed Watchdog Timer in LPC802?

1,044 Views
barbaramoraes
Contributor II

Hi! 

I wish to know what TWDCLK means, like in the case bellow:

pastedImage_1.png

When it talks about the minimum and maximum interval to watchdog, what means the TWDCLK, in yellow?

Best regards,

Labels (3)
Tags (3)
3 Replies

863 Views
barbaramoraes
Contributor II

Thank you very much guys!!!

863 Views
carstengroen
Senior Contributor II

According to the datasheet, the wdt oscillator is the "LPOsc" as far as I can tell.

And that has the following specs:

pastedImage_1.png

So the answer must be "approx 1 MHz"

863 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Barbara! 

The answer that Carsten Groen gave is correct. TWDCLK  is the clock of the Windowed Watchdog timer, that corresponds to the LPOsc. If you want to substitute TWDCLK  for the corresponding value you can use 1MHz.

Regards, 

Victor.