What is the state of IO during the period from power-on to boot on MCU LPC32?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the state of IO during the period from power-on to boot on MCU LPC32?

1,225 Views
Guestsun
Contributor II

What is the state of IO during the period from power-on to boot on MCU LPC32?

0 Kudos
Reply
2 Replies

1,212 Views
frank_m
Senior Contributor III

In a tristate mode, effectively off.

A common feature of all ARM Cortex M devices is, all peripheral units must be explicitely enabled (clock and power) to operate.
These peripherals are by default off at reset.

Very few exceptions might apply, like dedicated quartz input pins or JTAG/SWD pins.

0 Kudos
Reply

1,201 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Pls refer to data sheet of LPC32xx, the attribute of a pin is input(I), Output(O), bidirectional(I/O) , analog, power.

For the bidirectional I/O pin and Input pin, I suppose that the state of IO during the period from power-on to boot are in input mode, except for JTAG pins.

Hope it can help you

BR

XiangJun Rong

xiangjun_rong_0-1711606609838.png

 

0 Kudos
Reply