What is the recommended microcontroller series that replaces the LPC213x series?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is the recommended microcontroller series that replaces the LPC213x series?

ソリューションへジャンプ
1,264件の閲覧回数
kk7xo
Contributor III

It's my understanding that the LPC213x series is not recommended for new designs.  What series recommended for new designs has roughly equivalent capability (Memory size, speed, peripherals, etc.)?

ラベル(1)
0 件の賞賛
返信
1 解決策
1,148件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Albert,

The LPC21xx is Not Recommended In New Design, I suggest you refer to the LPC5411x and check if it meets your requirement.

LPC541XX | NXP 

But the LPC541xx does not have EMC module, so it can not hook with external SRAM, flash.

You can also check LPC51U68 for low cost solution:

LPC51U68 | NXP 

Hope it can help you

BR

XiangJun Rong

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,149件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Albert,

The LPC21xx is Not Recommended In New Design, I suggest you refer to the LPC5411x and check if it meets your requirement.

LPC541XX | NXP 

But the LPC541xx does not have EMC module, so it can not hook with external SRAM, flash.

You can also check LPC51U68 for low cost solution:

LPC51U68 | NXP 

Hope it can help you

BR

XiangJun Rong

0 件の賞賛
返信