What is the ADC absolute error of LPC54608J512?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the ADC absolute error of LPC54608J512?

Jump to solution
2,959 Views
Frank12345
Contributor I

What is the ADC absolute error of LPC54608J512? like LPC185x

Thanks

0 Kudos
Reply
1 Solution
2,914 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

By checking, For this part, Please use Eadj as absolute error , after gain and offset calibration(which is done in SDK ADC init function)

 

Have a nice day,

Jun Zhang

View solution in original post

0 Kudos
Reply
9 Replies
2,954 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

LPC546xx doesn't define ADC absolute error. Only Ed, El and Eo are tested.

If this data is necessary to you, please send me 

1. why this data is necessary to you?

2. your project name?

You can send these information with  community message to myself. if you don't want share it to public. thus I can check it internally.

ZhangJennie_0-1610947362400.png

Thanks,

Jun Zhang

0 Kudos
Reply
2,951 Views
Frank12345
Contributor I

Hi Jun:

 

 The absolute error should be the sum of the offset, gain, and integral non-linearity errors.

We need it to calculate the error rate of the ADC itself.

The project name is V8.

 

Thanks, Frank

0 Kudos
Reply
2,948 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

We can't know what V8 is.

Please let me know the scenarios of your application usage. thanks.

0 Kudos
Reply
2,944 Views
Frank12345
Contributor I

Our system provide a reference voltage to the external thermistor and then coonect to MCU ADC0INx.

Thanks.

0 Kudos
Reply
2,942 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

The application name can be, for example, "cash machine", "printer", "Traffic Control Light", etc.

What's yours application name?

 

0 Kudos
Reply
2,936 Views
Frank12345
Contributor I

Around View Monitor.

Thanks

0 Kudos
Reply
2,929 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Got it. 

I will check and keep you informed.

0 Kudos
Reply
2,915 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

By checking, For this part, Please use Eadj as absolute error , after gain and offset calibration(which is done in SDK ADC init function)

 

Have a nice day,

Jun Zhang

0 Kudos
Reply
2,912 Views
Frank12345
Contributor I

Got it, thanks.

Tags (1)
0 Kudos
Reply