What is "core 0" and "core 1" for the LPC55S66?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is "core 0" and "core 1" for the LPC55S66?

2,203件の閲覧回数
bob_nayar
Contributor I

I have noticed that when I set up a project in the MCUXpresso for the LPC55S66, the name of the startup file is called startup_lpc55s66_cm33_core0.c.

Similarly, when I start a project for the LPC55S66 in IAR, it asks me to choose between core 0 and core 1.

What is the difference?

Bob N

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,121件の閲覧回数
bob_nayar
Contributor I

Thanks, Jeremy.

Is there an SDK example project that uses both cores?

Bob N

0 件の賞賛
返信

2,121件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Bob Nayar,

Thanks for your reply.
1) Is there an SDK example project that uses both cores?
-- Please refer to the multicore_examples in the SDK library.

Have a great day.

TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

2,121件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Bob Nayar,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) What is the difference?\
-- The LPC55S6x/LPC55S2x/LPC552x device is the dual-Cortex M33 core MCU, it allows the demo project to be executed in either core 0 or core 1.

TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信