What are your experiences with the cable length of SWD wires?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

What are your experiences with the cable length of SWD wires?

2,679 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Martin84 on Thu May 22 15:25:51 MST 2014
Hi,

I want to flash and debug the Controller in my own application. Therefore I want to cut off the lpc-link from the target and use it outside the application for flashing the LPC11xx...

Can anybody tell me how long SWD cables can be? (I mean the 8-pin connection between the lpc-link and target)

Is it possible to get the µC flashed with a cable length of 30cm without additional bus drivers? Or should I just integrate the lpc-link in my own application too and program it over a usb cable?
标签 (1)
0 项奖励
回复
2 回复数

2,439 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Martin84 on Mon May 26 05:08:24 MST 2014
Thank you, R2D2.

I made a soldering mistake. After checking all connections it runs.

Regards, Martin
0 项奖励
回复

2,439 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Thu May 22 15:55:12 MST 2014

Quote: Martin84
Can anybody tell me how long SWD cables can be?



We are using SWD (4-wire Minimal Connection, 0.35mm twisted) with more than 30cm since several years without problems...
0 项奖励
回复