Vrefn in ADC equation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Vrefn in ADC equation

2,143件の閲覧回数
vaque
Contributor II

Hi;

I am working about a LPC824.

In UM10800.pdf at page 322 "Perform a single ADC conversion using a software trigger"  it says that The result of the conversion is (4095 x VIN)/(VREFP - VREFN). But I need to know why is that equation and not this other:

form3.png

The last one indicates a FS between Vrefp and Vrefn.

In this terms, the minimum LSB is:

form4.png

Can someone help me?

Regards. Daniel.

ラベル(3)
タグ(2)
4 返答(返信)

1,869件の閲覧回数
ckphua
NXP Employee
NXP Employee

For single end ADC input, the equation (4095 x VIN)/(VREFP - VREFN) holds since this is a simple ratio metric ADC.

Not sure how the equation with additional -VREFN comes into play.

0 件の賞賛
返信

1,869件の閲覧回数
vaque
Contributor II

@Chee Keong Phua, basically I need to know if result is always 0 for any value of Vin=Vrefn.

* The first previous equation is missing a parenthesis between (Vinn-Vrefn)

Thanks and regards. Daniel.

0 件の賞賛
返信

1,869件の閲覧回数
ckphua
NXP Employee
NXP Employee

When VIN less than or equal to VREFN, the ADC Count is  zero.

1,869件の閲覧回数
vaque
Contributor II

@Chee Keong Phua ok, thanks so much. Thus, the equation in UM10800.pdf at page 322 "Perform a single ADC conversion using a software trigger" is wrong. The good equation is this:

result = (4095 x (VIN-VREFN))/(VREFP - VREFN)

Thanks and regards. Daniel.

0 件の賞賛
返信