Content originally posted in LPCWare by jhd on Tue Dec 01 17:50:25 MST 2015
Hello,
Sorry if this post is not here, I did not know where to put it.
I need to build a voltage regulator and monitor current and voltage sense for LiPo batteries. 2S to 8S or 10S if is possible.
With this features:
V Input: from 7,4V up-to 50-60V
Current max.: 175A
V Out: 5V
Current Out: about 3A
And a 5V to 3,3V converter to supply providing of LPC54102, Bosch sensors, and other components in the pcb (all works to 3,3V), but other external periphericals works to 5V.
Best regards.