Voltage level I/O pins

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Voltage level I/O pins

644 Views
FruitSalad1
Contributor I

LPC55S16. Some output pins have 0,2V-3,3V, while others have 0,2V-2,0V. Why?

Have a look at my attachment.

regards

Labels (1)
0 Kudos
Reply
1 Reply

612 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @FruitSalad1 

The voltage range of output pins on an LPC55S16 microcontroller can vary depending on the specific pin and its configuration. Some pins are designed to work with a 3.3V logic level, while others are designed for a 2.0V logic level. This is due to the different internal circuitry and electrical characteristics of the pins.

BR

Hang

0 Kudos
Reply